This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMP102: Is it possible to apply 3.3V to SCL, SDA and ADD0 when powering off (V+=0V)?

Guru 26385 points

Replies: 6

Views: 251

Part Number: TMP102

Hi Team,

Is it possible to apply 3.3V to SCL, SDA, ADD0 and ALERT when powering off (V+=0V)?
I would like to know if TMP102 could be damaged or not in this case.

I believe it is possible according to the following absolute maximum ratings however would like to confirm just in case.



Best Regards,
Yaita

  • Hello Yaita,

    There is an update being done to the Absolute Max parameters for the device. And you are correct in the interpretation. When shutting down V+, the input pin voltage must not exceed the V+ voltage by 0.5V. Hence when V+ is 0V, the max voltage is 0.5V on the SDA, SCL, ADD0 and ALERT pins.

    Regards,

    Amit Ashara

  • Guru 26385 points

    In reply to Amit Ashara:

    Hi Amit-san,

    Thank you for your kind support.

    Regarding your comments, I believe the following red line should be modified in addition to absoute maximum ratings.
    Is my understanding correct?


    Best Regards,
    Yaita

  • In reply to K.Yaita:

    Hello Yaita,

    I would not agree on that. As long as the maximum parameters are not violated, it should be OK. Ideally the pull up supply and the V+ should be the same source, but based on the design it may not be possible always. I will check with a co-worker and confirm though.

    Regards,

    Amit Ashara

  • Guru 26385 points

    In reply to Amit Ashara:

    Hi Amit-san,

    Thank you for your support.
    OK, I will wait for your team's feedback.

    Best Regards,
    Yaita

  • In reply to K.Yaita:

    Hello Yaita

    I checked and my co-worked confirmed that as long as the variation is not more than +0.5V of the supply, the absolute spec will not be reached and the device can operate normally.

    Regards,

    Amit Ashara

  • Guru 26385 points

    In reply to Amit Ashara:

    Hi Amit-san,

    I think "not more than +0.5V of the supply" should be added just in case however I understand what you said.
    Thank you for your support!

    Best Regards,
    Yaita

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.