Hi,
I have two questions regarding the mmWave studio demo. Even though they are not entirely related, i thought of asking both in one post.
1. Where can i find more information about how the SPI/CAN switch works. As in, where it fits in the data path, etc. Because i noticed that it is important to have it in SPI for the mmWave Studio Demo. But works either way for the mmWave SDK Demo.
2. For the frame configuration, in the SDK user guide, it mentions that the Number of loops value "should be a power of 2". I indeed noticed that i run in to issues when reshaping the acquired raw data (through DCA1000) if the number of loops is not a power of 2. That was on a custom script we wrote. However, it seems to work with any value on mmWave Studio. Does mmWave Studio automatically just mask out the bits and just used the MSB if i give a value like 127?
e.g.127 = 0111 1111b being used as 0100 0000b = 64 ?
Thank you
Regards,
Navoda