This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: mmWave Demo Visualizer ADC Raw data running Matlab with IWR6843 and DCA1000 EVM

Part Number: IWR6843ISK


Hi,

I would like to enquire about the setting the configuration for mmWave Demo Visualizer as some of the parameters were different from mmWave Studio.

I would also like to check whether if I had set any setting wrongly with the default demo setting?

As I previously processed the data using mmWave studio + the matlab code (Mmwave Radar Device ADC Raw Data Capture). I'm able to get the result as shown in the application report.

http://www.ti.com/lit/an/swra581b/swra581b.pdf

However when I tried to set the same parameters using TI Visualizer, I couldn't seem to produce the same result as intended. 

Below are some of my parameters for mmWave Studio:

And this is my configuration using TI Visualizer

Configuration file for TI Visualizer

% ***************************************************************
% Created for SDK ver:03.03
% Created using Visualizer ver:3.3.0.0
% Frequency:60
% Platform:xWR68xx
% Scene Classifier:best_range_res
% Azimuth Resolution(deg):15 + Elevation
% Range Resolution(m):0.044
% Maximum unambiguous Range(m):9.02
% Maximum Radial Velocity(m/s):1
% Radial velocity resolution(m/s):0.13
% Frame Duration(msec):1000
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 60 359 7 57.14 0 0 70 1 256 5209 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
frameCfg 0 2 16 0 1000 1 0
lowPower 0 0
guiMonitor -1 0 0 0 0 1 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 1 1 1
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
sensorStart