Hi TI supporter ,
Please report TI your latest Toolbox4.3.0 released , the binary for 3d people counting demo is not workable.
I have stuck for long time for getting start with the dead EVM, due to the data port connection problem ,
Please give me the correct information that I can run these demo even the old version working that's ok and please help to fix it ASAP , and when will be fixed.
don't want to get such issue again in each trying of different version downloaded and evironment installed ,thanks.
My hand on EVM : mmWaveBoost+IWR6843ISK-ODS
and setup are as lists:
-EVM: mmWaveBoost card + IWR6843ISK-ODS (ES2 device)
-Toolbox: mmwave_industrial_toolbox_4_3_0
- GUI: mmwave_industrial_toolbox_4_3_0\labs\people_counting\visualizer
- Binary file: 3D_people_count_68xx_demo.bin @mmwave_industrial_toolbox_4_3_0\labs\people_counting\68xx_3D_people_counting\prebuilt_binaries
- Chirp : ODS_6m_default.cfg @mmwave_industrial_toolbox_4_3_0\labs\people_counting\68xx_3D_people_counting\chirp_configs
The issue as below :
1) The 3D People demo can't get point cloud data from data port after I send configuration file and the startSensor command .
2)Verified by using the TeraTerm , I have Opened both Data COM & config COM port ready .
When I send the chirp configuration command and send startSensor command , both Com ports were disconnected and disapearred in device manager.