Hello,
I am trying to debug an issue with an LMX9838 module I am trying to integrate into my product.
The problem I'm seeing is that the module will only power-up intermittently. According to the datasheet, after applying 3.3 V to the module's supply I would expect the Tx line to go high after some time. However, I don't see the Tx line go high.
I can fix the problem by applying 3.3 V from a bench power supply. I find that after I have powered it up once from the bench supply then I can successfully power the module up normally on my board. I suspect this is a problem with the power supply I'm using to drive the module. The regulator I'm using to power the module is the TLV70233.
Cheers,
--Mike