Hello all,
Can you recommend a passive RFID tag reader that i can interface with the TI RM48L ?
Thanks again
Giorgio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
Can you recommend a passive RFID tag reader that i can interface with the TI RM48L ?
Thanks again
Giorgio
Hello Giorgio,
What RFID technology are you looking to use? High Frequeny (HF)/NFC? Low Frequency (LF)? Ultra High Frequency (UHF)?
Hi Ralph,
thank you for your help, I really appreciate it.
Looking at the design, I could have a minimum distance between the reader and the antenna at about 5 to 6 cm.
Does the antenna help to extend the range of the reader? I mean, if I place the antenna inside the device, will it help to detect the rfid even if it is more than 1.7cm away?
Thanks again
Giorgio
Hello Giorgio,
That will also depend on the antenna size and output power of your NFC reader as well.
Just to give you a general idea, the TRF79xxA can output maximum 200mW of power w/ 5V input, and 70mW with 3V input. To maximize the range from the reader side, you will want to source the TRF79xxA with 5V.
For an idea on read range with a reader at 200mW output and a 55mm x 40mm antenna with a variety of RFID tag sizes please see this document: 5661.TRF796x EVM Read Ranges.pdf
Giorgio -
you may also want to consider looking at the Hercules LP + TRF BP
www.ti.com/.../launchxl-rm42
www.ti.com/.../DLP-7970ABP
Giorgio,
I agree with Josh on the LaunchPad and BoosterPack combo. It doesn't look like that DK board you linked has EM headers spaced correctly for the TRF7970ATB. The LaunchPad and BoosterPack would be a better combo.
Hello Giorgio,
No, the LaunchPad does not have connectors for the Target Board. You need to get the TRF7970A BoosterPack which is: http://www.ti.com/tool/DLP-7970ABP
There is no existing software example on Hercules for this, but you can port one of two firmware bases:
Fully Tested NFC/RFID Reader/Writer with robust error handling:
- App Note: www.ti.com/.../sloa227.pdf
- Firmware: www.ti.com/.../sloa227
Low footprint basic RFID Reader with basic error handling, designed for evaluation not production:
- Basic summary: e2e.ti.com/.../493678
- Firmware: www.ti.com/.../sloc297
Hello Giorgio,
I'm not familiar with Halcogen, so I am not sure about the different configurations. I don't think one has been made specifically for the DLP-7970ABP, but any configuration that would apply to BoosterPacks that follow the TI BoosterPack standards would work.