Part Number: THS4531A
Other Parts Discussed in Thread: THS4531
Hello,
I am contemplating on using THS4531A to build a Fully Differential Transimpedance Amplifier.
I realised that there is another component THS4531 which is quite similar to THS4531A.
I figured out the two components are different in following respect:
1. Harmonic Distortion@1kHz
2.Input referred offset voltage and drift
3. Input referred offset current and drift
Apart from these, are there any other differences in the two components ?
Is there any restriction on using THS4531 instead of THS4531A ?
Is there any document telling the difference between THS4531 and THS4531A ?
regards,
Ashish