Other Parts Discussed in Thread: SN74LVC2G34 FAQ: Logic and Voltage Translation > Output Parameters >> Current FAQ
There are a few issues with trying to determine a maximum capacitive load for a standard CMOS logic device.
First is propagation delay…
Part Number: MSP430F67771A Other Parts Discussed in Thread: MSP430F6777 , MSP430F67771 , , MSP430F6777A
Hello,
Greetings. and sorry for the trouble. I could not find any data showing the difference between MSP430F6777 and MSP430F67771
Can any one…
Part Number: OPT3001 Other Parts Discussed in Thread: OPT3002 OPT3001 measurement level is 0.01lux to 83k lux, and OPT3002 measurement level is 1.2nW/cmcm to 10mW/cmcm.
What is the difference between these measurement levels?
FAQ: Logic and Voltage Translation > Quality and Manufacturing >> Current FAQ
In short, there will be no difference between a device labelled SN74xxG4 and SN74xx.
Historically, G4 and E4 suffixes meant that the devices were rated to be "Green" or…
Other Parts Discussed in Thread: TUSB1002A I am implementing a USB 3.x signal redriver to help with signal integrity issues. I understand that a redriver provides equalization to the signal path but what losses are affected by this equalization?
Other Parts Discussed in Thread: TUSB8044 , TUSB8041A , TUSB8043 , TUSB8042 , TUSB4020BI , TUSB8020B , TUSB8041 , TUSB4041I I have implemented a USB Hub with four USB 3.1 Gen / USB 2.0 ports using TUSB8044 however the downstream ports don’t work when…
Question:
Interrupts are blocked in my application when when the compiler uses the RPT (repeat a single instruction). How can I limit the number of times RPT is applied to an instruction or tell the compiler to not use RPT so that interrupts get through…