Part Number: UCC5881-Q1 Other Parts Discussed in Thread: UCC5880-Q1 ,
UCC5881-Q1 is TI’s latest programmable isolated gate driver, offering pin-to-pin compatibility with the exact same package and pinout as UCC5880-Q1. This enables designers to keep…
Part Number: AM2612
Hi ASM team,
I get the following error after trying to build a simple GPIO toggle program on a clean install of the 10_02_00_15 SDK. Have we seen this before?
All the best,
Ethan Cope
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG , TAD5212
Mcasp buffer order
To be short, in case of multiple serializers used in one Mcasp, the samples are placed interleaved by slot not frame by default. (Please check the "12.1…
Part Number: J722SXH01EVM
Tool/software:
How do I use the Fusion2 board with the J722SXH01EVM ?
When I try to run the single camera demo, I see the following error:
[MCU2_0] 76.844004 s: Error writing 0x01 to de-serializer(0x3d) register 0x4c…
Part Number: MSPM33C321A
Tool/software:
When MSPM33 enter a state where CCS is unable to connect to M33 core, follow the below procedure to implement Factory Reset.
CCS version >= CCS v 20.4.0.5
Step 1 - Launch project less debug
Step 2 -…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TXE8148 , TXE8116 , TXE8124
Tool/software:
FAQ: Logic and Voltage Translation > SPI I/O Expanders >> Current FAQ
This FAQ describes 6 key spec's for I/O expanders.
These specs include: …
Part Number: TDA4VM
Tool/software:
I'm using the TDA4VM Linux or Linux+RTOS 8.6 SDK. What parameters or patches are available to be enable I-frame period and IDR frame period?
Part Number: AM62A7 Tool/software: Currently on the AM62A TI EVM, we have a OSPI Serial NAND Flash from Winbond.
The flash is: W35N01JWTBAG
Let us understand how the BBM is done with respect to some specific registers.