Part Number: BQ25883
The BQ25883 and other devices in the family have a Soft Start Feature on Vsys output. This can be seen in datasheet fig77 that Vsys has a slow ramps-up. The Soft-Start feature at power up is noted in par 8.3.3.4.
Slow rate of…
Part Number: BQ25171-Q1 Other Parts Discussed in Thread: BQ25172 , BQ25173-Q1 , BQ25173 , , BQ25170
This home page is for common questions in relation to the BQ25171-Q1, BQ25173-Q1, BQ25170, BQ25172, BQ25173
FAQs
-------------------…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329A , MCF8329HS
MCF8329HS: Advanced Motor Control IC with Enhanced Performance
The MCF8329HS builds upon the proven MCF8329A platform, delivering enhanced motor control capabilities and…
Part Number: AM2612 Other Parts Discussed in Thread: UNIFLASH
Hi Team,
Customer is programming AM2612 on their own board, but it not works through Uniflash, could you please help to check the log and point out next step? Thanks.
Uniflash log.…
Part Number: AM2612
Hi experts, I see that the AM26x devices support Inter-Processor Communication between multiple R5F cores and include a mechanism to maintain shared memory across cores. What is recommended for my multi-core applications? When do…
Part Number: MSPM33C321A
Per ARM architecture, VTOR must be aligned to:
Alignment = Power of 2 ≥ (Number of vectors × 4)
For MSPM33C321A:
- ICTR register = 1 → Hardware supports 53 external IRQs (IRQ0- 52 )
- Total vectors = 16 (system exceptions…
Part Number: INA236 Other Parts Discussed in Thread: INA3221 , INA209 , , INA228 , INA237
I want to use the ALERT pin of a digital power monitor, what should I pay attention to?
Part Number: AM2434
While the existing OSPI driver implements XIP mode functionality, the default Flash parts (S28HS512T and S25HL512T) available on AM24x, AM64x, AM62x, and AM275x boards, do not support Read-While-Write (RWW) operations or multi-bank…
Part Number: TPS3842
I need to monitor and sequence 3 power supply rails. The main bus voltage in my design is 12V, followed by LDOs for 5V, 3.3V, and 1.8V. Can please provide the simplest solution? Also board size is very limited so I need smallest…