Other Parts Discussed in Thread: UNIFLASH , MSP430FR2310 , MSP430FR2311 , MSP430FR5962 , MSP430FR5964 , MSP430FR5992 , MSP430FR5994 There is an issue with some of the device support files for MSP430 that will impact some users of UniFlash and CCSv9.1…
Part Number: TPS23758 Other Parts Discussed in Thread: TPS23755 ,
What are the differences between TPS23758 and TPS23755? TI's compare tool show them to be the same.
For starting new project, which part is recommended?
Hello,
Many of the TLV320AICxxxx and TLV320ADCxxxx datasheets refer to "standard" and "fast" I2C modes. Can you confirm which speeds these correspond to?
Part Number: AWR1843 Recently, we have received questions related to detecting static objects at near range (~ 40 cm). This thread will discuss some of the specific details related to this type of detection.
Readers are invited to ask more questions…
Yes, it is. The changes from LIN 1.3 to LIN 2.0 and above are purely LIN protocol changes. The physical layer transceiver definition was not affected directly or through the protocol changes.
For more information on the changes to the LIN specification…
Other Parts Discussed in Thread: SYSBIOS Hello Everyone,
The newest Industrial Toolbox 3.4.0 is now available on the TI Resource Explorer. Updates are listed below,
Lab/Experiment/Chirp Name
Changes
LAB: Vital Signs - 68xx…
Other Parts Discussed in Thread: LM833 How do I design Low Noise & Low Distortion Headphone & Small Signal Audio Amplifiers?
Headphone Amplifiers
On-Chip Thin Film Resistors Enable High-Performance Audio Circuitry – SBOA312
Stabilizing Difference…
Yes, they can. 3.3V CAN transceivers are designed to have their recessive level, dominant and recessive thresholds such that they will correctly transmit and receive messages from either a 5V or a 3.3V CAN transceiver. Within the 3.3V CAN transceiver…