Part Number: J722SXH01EVM
Tool/software:
How do I use the Fusion2 board with the J722SXH01EVM ?
When I try to run the single camera demo, I see the following error:
[MCU2_0] 76.844004 s: Error writing 0x01 to de-serializer(0x3d) register 0x4c…
Part Number: MSPM33C321A
Tool/software:
When MSPM33 enter a state where CCS is unable to connect to M33 core, follow the below procedure to implement Factory Reset.
CCS version >= CCS v 20.4.0.5
Step 1 - Launch project less debug
Step 2 -…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TXE8148 , TXE8116 , TXE8124
Tool/software:
FAQ: Logic and Voltage Translation > SPI I/O Expanders >> Current FAQ
This FAQ describes 6 key spec's for I/O expanders.
These specs include: …
Part Number: TDA4VM
Tool/software:
I'm using the TDA4VM Linux or Linux+RTOS 8.6 SDK. What parameters or patches are available to be enable I-frame period and IDR frame period?
Part Number: AM62A7 Tool/software: Currently on the AM62A TI EVM, we have a OSPI Serial NAND Flash from Winbond.
The flash is: W35N01JWTBAG
Let us understand how the BBM is done with respect to some specific registers.
Part Number: PROCESSOR-SDK-AM62X
Tool/software:
In MCU+ SDK, during Flash Initialization, we read the device id and manufacture id.
Most common failure is " Unable to read Flash ID... "
Let us understand what parameters does the API Flash_norOspiReadID…