Part Number: BQ25188
The BQ2518x resets its R/W registers to the default values whenever a reset condition occurs. This can happen due to watchdog timers, power-on reset (POR), or a software-initiated reset.
Watchdog timer
The BQ2518x includes a…
Part Number: BQ25188
Power Dissipation
The BQ2518x is a linear charger with power path. Power path is a feature that allows the BQ2518x to power the system from the input source while simultaneously charging the battery. The back-to-back input FETs…
Part Number: AM275-FREERTOS-SDK
The FreeRTOS SDK and MCUPlus SDKs both contain additional libraries, such as DSPLib. These libraries by default are not meant to run within CCS projects directly, but rather to be compiled with cmake.
It is possible…
Part Number: AM625
BINMAN tool is currently used to sign u-boot binary in Linux SDK, where the signing key is locatable under Linux SDK folder. There's a need to use the signing key stored in the external secure key server when switching to the production…
Part Number: TDA4AEN-Q1
Example explaining the steps of combined app image with WKUP R5F and MCU R5F in J722S without HLOS
https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j722s/latest/exports/docs/mcu_plus_sdk_j722s_11_01_00_15/docs/api_guide_j722s…
Part Number: TDA4VH
Support for user-mode host-id for A72/A53 HLOS running user-mode drivers: ==============================================================
Before the SDK 11.2 release, the UDMA resource allocation utilized elevated privileges for…
Part Number: AM2432 Other Parts Discussed in Thread: UNIFLASH
The ENETFOTA example demonstrates how Ethernet can be used to transfer a new application image from a host PC to an AM243x/AM64x device that is currently running an older application image…
Part Number: TDA4AEN-Q1
Sporadic hang in RPMessage_ProcessAnnounce API in ipc echo test while running with safeRTOS on SDK 10.1 , it was observed even with ctrlmsgTask keeping at high priority.
Part Number: TDA4AEN-Q1
FLS APP INDAC example is not showing performance numbers on SDK 11.0. How to get performance numbers similar to other jacinto devices ?