Part Number: LMH1239 Other Parts Discussed in Thread: LMH1297
Tool/software:
Hello SDI engineers and LMH enthusiasts,
Figure 1 - 3:5 for SDI
In this E2E FAQ, I will be discussing GND plane layout best practices for SDI designs. In cable driver…
Part Number: AM625 Other Parts Discussed in Thread: AM6442 , DS160PR810 , AM67
Tool/software:
Hi TI Experts,
Do you have recommendations on using the IBIS model?
Part Number: PROCESSOR-SDK-AM62X
In Linux kernel 6.12, we remove the separate PRU RPMsg (RPMessage) driver, and use the generic RPMsg driver instead. However, the changes were not complete in time for Linux SDK 11.0. This means that PRU RPMsg does not…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: AM62P , AM62L , SK-AM64B , SK-AM62B-P1 , SK-AM62-LP , SK-AM62A-LP , SK-AM62P-LP , TMDS62LEVM , AUDIO-AM62D-EVM , SYSCONFIG
Tool/software:
The objective of this FAQ is for someone with…
Part Number: AM2612 Tool/software: Hi TI experts,
I am using CCS v12.8.1, MCU_PLUS_SDK for AM261x. If I try to import any example from AM261x MCU+ SDK, I get the following error:
Even if I try to create a new Project from scratch, it says " Device…
Part Number: MCU-PLUS-SDK-AM261X Other Parts Discussed in Thread: LP-AM261 , SYSCONFIG Tool/software: Hi TI experts,
All ADC2 values output as '0' on AM261x.
Example output on is adc_multiple_soc_epwm_am261x-lp_r5fss0-0_nortos_ti-arm-clang and on…
Part Number: AM2612 Tool/software: Hi TI experts,
I am using the AM261x-LP board and running into the following USB issues:
I tried running the SBL DFU application via the dfu-util tool provided. I am not able to get the device to enumerate after…
Part Number: UCC27714
Tool/software:
There are numerous 600V half-bridge gate drivers available in 8 pin SOIC packages and also higher pin count 14 pin packages. With the 8 pin SOIC package, only the basic half-bridge gate driver functions are available…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH , J784S4XEVM Tool/software: I'm seeing issues with the display experiencing sync losts when running the TIDL AVP demo. How do I balance the transaction loads and priorities so that the DSS…