FAQ: TPLD > Current FAQ
Customers can order devices for production through InterConnect Studio (ICS). TI can program devices (at no additional cost!) before shipping with the submitted design if the order quantity is one reel or more (3000 units). …
FAQ: TPLD > Current FAQ
TPLD uses Floating-Gate One-Time Programmable (OTP) technology to program its parts, as opposed to other Non-Volatile Memory techniques such as eFuses or AntiFuses, or Volatile Memory technologies such as EEPROM or RAM.
Floating…
FAQ: TPLD > Current FAQ
TPLD stands for TI Programmable Logic Devices . These devices are a family of programmable logic devices integrating multiple digital and analog functions into a single small package.
Top TI Programmable Logic FAQs
What is TPLD?
Does TPLD have memory? What kind of memory does TPLD use?
Can TI program TPLD for me?
Can a third party program TPLD for me?
Can I permanently program TPLD in-system or in production myself?
What…
I am using an AM62x, AM62Ax, AM62Px, or AM64x.
I want to run the MCU+ SDK's ipc_rpmsg_echo_linux example [1] to communicate with the Linux kernel rpmsg_client_sample driver [2]. I am using Linux SDK 10.0, 10.1 (Linux kernel 6.6), or Linux SDK 11.0 …
Part Number: AM6442
Tool/software:
(Customer Query)
Hi TI Experts
We are in progress for the Rev.B changes for the V2 SCC schematic and we have made few changes related to the reset circuit for which we need input/confirmation from TI.
In…
Part Number: MCU-PLUS-SDK-AM261X Other Parts Discussed in Thread: DP83826-EVM-AM2 , SYSCONFIG Tool/software: Hi Experts,
I am using AM261x-LP with MCU_PLUS_SDK for AM261x v10.00.01.10. For CPSW Based networking examples, I am unable to configure MII…
Part Number: DP83TC812S-Q1 Tool/software: Hello,
Here is a summary of available information about RGMII Shift and Align mode for our DP83TC81x devices:
A minimum of 1ns setup and 1ns hold time must be maintained at the input of the receiver…