Part Number: F29H850TU
When i load a crypto example from the SDK through the ccs debugger and run it from the same, it doesn't work until i give an XRSn or a PORSn.
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74720-Q1 , LM74800-Q1 , LM74900-Q1 , LM74930-Q1 , LM74502-Q1 , LM74500-Q1 , LM74912-Q1
What is the need of TVS+ in bidirectional or unidirectional diode when used with ideal diode controllers…
Issue
When running Automatic Mixed Precision (AMP) with TIDL, users may observe: - AMP runs for an extremely long time without completing - Hundreds of gigabytes of intermediate trace files accumulate on disk
Root Cause
AMP works by running the…
Overview
This guide covers a component-level upgrade, replacing the c7x-mma-tidl and mmalib packages inside an existing SDK 11.00 build environment, without fully migrating to SDK 11.02. It also updates the targetfs runtime libraries (onnxruntime, TFLite…
Part Number: AM625 Other Parts Discussed in Thread: AM62P-Q1
HI TI experts:
I am designing a custom board with UART, MCSPI and MCAN interfaces.
Please let me know if you have any design recommendations.
Regards,
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: SYSCONFIG
Please share the details required to update board configuration to be able to test ECC on the Main NAVSS inaccessible endpoints from the MCU R5F.
Part Number: AM2634-Q1 Other Parts Discussed in Thread: UNIFLASH
Hi Expert,
I'm experiencing long delays when loading images into external flash using UniFlash. The tool spends the majority of its execution time initializing and setting up the environment…
Part Number: AM625 Other Parts Discussed in Thread: TMP100 , AUDIO-AM62D-EVM , SK-AM62A-LP , SK-AM62B-P1 , SK-AM62-LP , SK-AM62P-LP , TMDS62LEVM , TMDS64EVM
TMP100 is an I2C/SMBus interfaced digital temperature sensor that is available on the EVMs…
Part Number: MSPM33C321A Other Parts Discussed in Thread: SYSCONFIG ,
1. Background
Since the LP-MSPM33C321 features an onboard OLED display, you can display images and animations, such as in [FAQ] MSPM33C321A: How to play video 'bad apple' at LP…