Part Number: TDA4AL-Q1 Hi ti
emmc startup time in SBL mode is 30s, but emmc startup time is 2s in SPL mode, please help me check.
emmc startup time in SBL mode log:
SBL Revision: 01.00.10.01 (Oct 8 2023 - 12:50:20) [2023-10-08 14:23:56.774] TIFS ver…
1.
Results below are for 12 Cells. The voltage in my pervious comment of 55.23V was setup for 14 Cells. The LD voltage does not match the Stack voltage.
FETs OFF
FETs ON
2.
Callibration:Voltage:Pack Gain register = 33845
3.
ADC results - tested first…
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: 5-8-LOGIC-EVM Hi,
I am trying to evaluate the SN74LVC2T45 and the generic 5-8-LOGIC-EVM is the recommended TI tool. However I do not see any diagrams in user guide to tell me how the layers are…
Hi Nilabh,
After I change this file, it works.
Thank you for your help.
Hi Jiri,
This issue is occurred when we only change EEPROM driver without modifying any CUST_drivers.c. Modifying CUST_drivers.c aim at trying to workaround and finding the reason…
Hi Jay,
I tested the SDK 9.0 prebuilt image (tisdk-default-image-am64xx-evm.wic.xz) on AM64 GPEVM, the PCIe RC is enumerated. Please compare with the SDK prebuilt to see what is missing in your setup.
root@am64xx-evm:~# uname -a
Linux am64xx-evm 6.1…
The following modifications have been done for SPI connection between FMC and AFE and FMC and LMK
SPIA connection between FMC and AFE8030 chip
Populate R424, R420, R408, R405 with 0 ohm resistors (footprint is 0201)
Populate R76, R75, R74, R73 with…
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: TDA2
HI TI erperts:
有两个问题帮忙解答 下
1 参照MMWCAS-DSP-EVM设计级联雷达处理板中,能否将DEMO板中的60 pin MIPI JTAG口换成14 pin的JTAG仿真器标准座子? 即去掉EMU信号,如果可以需要哪些注意事项?
2 换成14 pin的JTAG仿真器标准座子, 可能会有哪些影响?比如哪些功能不支持,或者速度变慢等。
Hi Gabriel, I did a quick test and it does not show a deviation of ±3℃ at room temperature. See attached. internalTemp_deviation_no_calibration.xlsx My testing conditions are with the device at relax (no charging/discharging). Temperature changes when…
Hi Masae Kawakami,
Welcome to the E2E forum! The SPI engine is built into the M0 core and for communication you will have to follow the datasheet information by following the command codes shown in Table 5. There isn't any additional documentation that…
Hafiz,
There does seem to be some issue in that updated firmware, but it may take some time to track it down. I have attached the firmware that is loaded at manufacturing. This seems to fix the issues I was seeing as well. Please try reverting back to…