Part Number: TPS53317A Tool/software: ATTENTION: This is the ONLY attempt by IBM to secure information regarding the use of the newly added SVHC(s) in deliverables supplied by your company to IBM. If no response is received, IBM interprets your silence…
Hi Stephen,
My point is that the user space applications should not rely on the gpiochip IDs or gpio pin numbers which vary from kernel to kernel or even platform to platform. To completely decouple the applications from kernel, gpio pin names should…
Hello Monica,
We use the isolator for two reasons:
1- To protect the MCU communication lines from any EMI/EMC damage like transients.
2- Is because most MCUs communicate with 3.3V logic. Our BQ device communicate with 5V logic.
As long as you can communicate…
Part Number: EVM430-CAPMINI Other Parts Discussed in Thread: MSP430FR2512 , , MSP-GANG , UNIFLASH
Tool/software:
I am trying to replicate the Captivate HID bridge (MSP430F5510IRGZT) adaptor part of the EVM430-CAPMINI touch evaluation module. It would be…
Hi Krunal, When the system starts, I first get the TI splash, then Weston and then it tries to boot my app. When I disable the splash, weston and my app service, I still get the Arago terminal (maybe this is the one locking the screen, don't know how…
Hello Alex,
The ADS1231 is the best alterative device to the AD7780. Please find the comparison of the two devices below.
Competitor
TI
Parameter
AD7780
ADS1231
Description
24-Bit Pin-Programmable Low Power Σ−Δ ADC…
Hi,
we use video mode is sync pulses .RGB888 ;
DSI clock is continuous mode;
DSI rate is 1984*792*60*24/4/2=282.8M
PCLK is 1984*792*60=94.3M
The data we obtained at the 948 output is different from what we set at SOC:
getfor948
fm_value:32914
lvds_clk_in…
Hello Christophe,
The schematic is from the reference design TIDA-01487 reference design @ TI.com . Unfortunately, there is no physical board or orderable part for this design since reference designs are for reference only. The link does have all the design…
Thanks for responding.
Clemens Ladisch said: How are you trying to measure the hysteresis?
I'm just looking at the scope. I see from the scope image that the rise and fall times for the output are about 20ns. Is that what you would expect from this table…
Part Number: LM5170EVM-BIDIR Other Parts Discussed in Thread: LM5170-Q1 , LM5170 Tool/software: Hi,
We have design the board as per EVM schematic. However while testing we could not enable brake circuit. As per instructions in the EVM user guide , we Kept…