Part Number: J722SXH01EVM Other Parts Discussed in Thread: AM67A Tool/software: Hi,
we are having trouble toggling the GPIOs on the AM67A EVM. We've tried three GPIOs so far:
Pin17 on J33 (22Pin CSI camera port): GPIO0_15
Pin18 on J33 ( 22Pin CSI…
At this point, I can share the tp6(tp5, tp8 also) logged data of a similar case which was captured during the diagnosis, yet not the scope image.
mabs test point-14MAR23.xlsx
Juhyun Kim said: but I just ended up with different and weired result as below.
I am not sure why you have the dark output YUV image. Your share raw image looks OK to me.
You may try the latest python script in the link below as I have updated it recently…
Part Number: AFE7950 Tool/software: This is about the JESD parameter LMFSHd.
The AFE7950 has 8 lanes and 4 converters for TX/RX. The resolution is 14 bits.
If LMFSHd=48810, why is F=8?
There are 2 octets (14 bits) per converter, so if M=8, I think F…
Hi Bin san,
Thank you for your reply.
I got following trace log when the problem occurred.
Aug 11 06:52:24 am335x-evm kernel: ------------[ cut here ]------------
Aug 11 06:52:24 am335x-evm kernel: WARNING: CPU: 0 PID: 22742 at drivers/usb/musb/musb_host…
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: 5-8-LOGIC-EVM Hi,
I am trying to evaluate the SN74LVC2T45 and the generic 5-8-LOGIC-EVM is the recommended TI tool. However I do not see any diagrams in user guide to tell me how the layers are…
Dear Prashant,
For flashing the rootfs image which image i have to include that new generated rootfs.ext4 right.But it showing error. suraj@suraj-HP-Laptop-15s-fr2xxx:/opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/DFU_flash$ sudo python3 dfu_flash…
Hey Manoj,
The only other way I can think of for verifying that the file is transmitting correctly would be to scope the bus, connect a logic analyzer with CAN support, or a CANanalyzer during file transmission. Have you attempted to manually send one…
Hi,
It's a custom board but based on the AM64x EVM as a reference design and it uses the same bootmode buffer implementation for example.
root@am64xx-evm:~# uname -a Linux am64xx-evm 6.6.32-ti-01287-g6de6e418c80e-dirty #1 SMP PREEMPT Fri Jul 26 14…