Part Number: ADC3444 Other Parts Discussed in Thread: , THS4541 Hello,
I would like to know if I need a ADC driver (unit gain or more) for ADC3444 driving because there is IF crystal filter (single-ended, R=3000 Ohm//1pF) just before ADC.
Is the ADC driver…
Part Number: ADC3444 Other Parts Discussed in Thread: ADC3244 We think that it is fine, but there seems to be a bit of an issue with the ADC344x Datasheet SBAS670B –JULY 2014–REVISED APRIL 2017.
Table 7.12 seem to have a couple of typo’s…
Part Number: ADC3444 Does the ADC3444 consists of the frame clock pattern? how to rearrange the frame clock while coming from the pcb? is there any application notes available related to this topic? thanks in advance
Part Number: ADC3444 We see that the datasheet says that synchronisation could cause glitching on the clock:-
On the ADC344X we have two output clocks: DCLK and FCLK. It is not clear from the datasheet which of the clocks is affected by the Synchronisation…
Hi Amy,
Kindly check the below high-level block of ADC3444 with isolation amplifier AMC3301.
/resized-image/__size/1000x1000/__key/communityserver-discussions-components-files/73/ADCC3444_5F00_Block_5F00_Diagram.JPG
Could u please review and confirm ca…
Hi Nick I'm not familiar enough with the Sitara evaluation module to know what high speed ADC EVMs might be compatible. I am going to re-direct this question to the TMDSEVM572x experts to see if they can provide any additional information regarding…
Part Number: ADC3444
Dear Forum members,
Could you please comment on the following?
From the datasheet: SBAS670B – JULY 2014 – REVISED APRIL 2017
Whilst keeping note (1) above in mind.
Assuming AVDD = 1.8V the maximum input voltage should…
Part Number: ADC3444 Other Parts Discussed in Thread: ADC3442 , Dear Forum members.
Could you please comment on the following?
Is there a graph available detailing the power consumption on the analog and digital rails versus the sample rate?
For example…
Part Number: ADC3444
Hi everyone,
Please help me with this question:
I got a customized board using an lvds ADC adc3444 and Xilinx 7 serial. I found the DCLK_p/n and FCLK_p/n are not connected to MRCC or SRCC, instead, to common lvds…
Part Number: ADC3444 Dear all,
I am a little bit confused about the 2-Vpp input swing.
From the datasheet, "... The ADC344x analog signal inputs are designed to be driven differentially. Each input pin (INP, INM) must swing
symmetrically between …