Part Number: ADS1220-EXCEL-CALC Other Parts Discussed in Thread: ADS1158 , ADS127L11 Hello I am looking for TINA spice or PSpice .LIB files for the ADS127L11, or ADS1158 or any of the similar ADCs which use Delta Sigma modulation.
Do these files exist…
Part Number: ADS1220-EXCEL-CALC Other Parts Discussed in Thread: ADS1220 , Normally for SAR ADC input. A R/C charger bank is required. When consider the R, does that include the output impedance of the amplifier(if use an amplifier to drive the SAR ADC…
Part Number: LMG5126 The maximum switching frequency for my design on WEBENCH with the LMG5126 will only go to 800khz max. The CALC excel sheet allows me to go to 2000 or higher, but there is no efficiency chart in the excel sheet, which is different…
Part Number: ADS1261-EXCEL-CALC-TOOL Other Parts Discussed in Thread: ADS1261 , ADS1261EVM , DELTASIGMAEVAL-GUI HI Team,
Below is the setup:
Hardware Setup:
Board: ADS1261 EVM
Sensor: 3-wire PT100 RTD
Wiring:
Red wire → AIN0
White wire…
Part Number: ADS124S08-EXCEL-CALC-TOOL Other Parts Discussed in Thread: ADC-RTD-CONFIG-CALC , Dear Support,
While using the RTD Calculator for my circuit, I noticed a behavior that I am unable to explain.
The accuracy calculated by the tool is exactly…
Part Number: LM2576HV Tool/software: Hi can you provide a calculator for LM2576HV negative output in Excel sheet format?
I appreciate your reply
Best Regards
Naji
Part Number: LM25145 Other Parts Discussed in Thread: LM5146 , LM5145 Tool/software: Team, I hope you are well.
The calculation Excel sheet for this device is missing here : LM25145DESIGN-CALC Calculation tool | TI.com
Could you please provide the…
Part Number: TMS320C6655 Tool/software: Hi Experts,
Could you please send me the DDR3 Register Calc excel file that used in C6655/C6657 EVM?
i want to verify these parameters which depends to DSP SoC configuration
Part Number: TPS25983 Hello team,
I am not able to change the cell value of NRETRY (D19) on TPS25983-CALC .
It says this sheet is being protected, and asks for a password. Could you give me password to unlock the protection?
Best Regards, Kei…
Part Number: ADS124S08-EXCEL-CALC-TOOL Other Parts Discussed in Thread: ADS124S06 Dear Sir / Madam,
If ADS124S06 is selected on the Register Map sheet, AINCOM cannot be selected with MUXP or MUXN.
Why?
Thanks and best regards,