Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131M08 Hello Sir,
I wanted to measure following parameters for meterology project.
1) Voltages (L1-N, L2-N, L3-N, N-PE)-When neutral is present
2) Voltages (L1-PE, L2-PE, L3-PE)- When Neutral…
Part Number: ADS131M06 I appear to be having a problem setting up an ADS131M06. I can read back the registers I set but there appears to be no difference in the output.
I've checked the signal with an oscilloscope to check the edge quality and with a…
Part Number: ADS131M06 The impedance matching of the CLK waveform is not good for my SPI communication signal, and it seems to be a count error of the data signal.
Question (1): Does the ADS131M06 SPI input port have features like schmit trriger?
Question…
Part Number: ADS131M06 I'm using ADS131M06 ADC (with a STM32G474), and having issues setting the PGA gain 8x and above.
I have multiplexed all channels to the positive internal test signal, which I believe is designed to read the same ADC value irrespective…
Part Number: AM2432 Other Parts Discussed in Thread: ADS131M06 ,
Hi Expert,
When an external ADC chipset(ADS131M06) is connected to AM2432, this external ADC chipset requires an external master clock in the range 4MHz~10MHz. I plan to use the generated clock…
The SCKL from the LPAM243 is just broken somehow. I don't have another board to tell if its a problem with my board or with their design, but the waveform is properly scaled at 1MHz, just not the 25MHz needed for this ADC. I am currently working on getting…
Part Number: ADS131M06 Hi Team, May I ask for help? Our customer have a concern: Would you tell me please if I must match the impedance of the ADC input which can be ( 1M or 330KOhms ) to the voltage divider impedance? I hope you can help as clarify the…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS124S08 Hello Guys,
Good day.
Our customer is designing a board that requires 12 ADC channels, 6 are differential and 6 are single ended. Can the ADS131M06 be configured to support the 6 single…
Part Number: ADS131M06 Hi Ryan,
Sorry i was away for Long time and busy with other things.
Actually i am sensing AC Voltage of 540V with upper resistor of 900K and Bottom resistor of 2K.
so at ADC i am getting 1.2V when 540V is applied.
For continuous…
Part Number: ADS131M06 Hi,
Can you please help me in understanding noise level lost in conversions?
I wanted to measure 300VAC with the resolution of 1V
how i will make sure that with this ADC, I will achieve this resolution.
Regards,
Deepak