Other Parts Discussed in Thread: ADS5463-SP , ADS5463 , DAC5675 Hi,
We are interfacing the digital output side of a ADS5463-SP directly to Xilinx Virtex-5 LVDS receivers. Our plan is to also clock the ADS5463-SP at a ~150MHz rate from an output structure…
Other Parts Discussed in Thread: ADS5463-SP Hi,
Are the two RESERVED pins (31 & 35) totally unconnected within the ADS5463-SP package, or are they attached to some internal voltage potential, test point, or other logic?
Other Parts Discussed in Thread: ADS5463-SP On page 18 of the ADS5463-SP datasheet it states that the DRY signal should be used to capture the DATA out of the ADC. However, when I look on page 9 of the datasheet and review the timing information it appears…
Other Parts Discussed in Thread: ADS5463-SP Hi,
Does any know where I can get information about ADS5463-SP SEE (Singe Event Effects) ?
I read this datasheet and its only specifies that TID is 100 Krads.
Thank you
Other Parts Discussed in Thread: ADS5463-SP , CDCM7005-SP Hi Team,
I was calculating the clock jitter at the input of ADC, ADS5463-SP. The customer is using an XO with period jitter (1 sigma) of 25 ps rms and 12K to 20M jitter of 0.3ps rms.
They…
Part Number: ADS5474-SP Other Parts Discussed in Thread: ADS5463-SP , ADS5400-SP , ADS5444-SP Hello,
Can you check the characterization data for the ADS5474-SP?
One of our customers plans to running this converter at 200MSPS. However, all the current…
Both the ADS5444-SP and ADS5463-SP were released in 2008 and both have flight history. The ADS5463-SP is more popular and is also available as RHA 5962R0720802VXC.
Anton
Hi Kirby,
A while back you had suggested using the THS4513 (or THS4511) amp to drive an ADC. Our ADC selection has changed to the TI ADS5463-SP. On page 17 of the ADS5463-SP data sheet an example circuit for using the THS4509 to drive the ADC is shown…
Other Parts Discussed in Thread: ADS5463-SP , ADS5444-SP , ADS5463 Hello,
I am considering using the ADS5444-SP or the ADS5463-SP ADC converters in a space application. To limit power, I would like to power up the devices only when I have a signal event…
Other Parts Discussed in Thread: ADS5463-SP , ADS5444-SP Hello,
I have a low power, high-speed application in which I need to sample at 250 MHz and want to conserve power by shutting off the voltage to my ADC until there is a signal of interest. I'm…