Other Parts Discussed in Thread: ADS7861 , TXS0108E Hi.everybody.
I am using an alteral DE2 board to obtain result from a ADC (ADS7861). Since the DE2 output voltage is 3.3V only, i use a voltage translator, TXS0108EPWR for the conversion from 3.3V to…
Hi Daniel,
Thanks for your question on the ADS7863! This is something I've helped others with in the past on the earlier versions of this device like the ADS7861 and ADS8361. The CONVST and RD inputs do need opposite edges of the SCLK to get everything…
Hi Alberto,
You are correct - the ADS8361 cannot provide data faster than 125KSPS using the single serial output mode. The ADS8363EVM is compatible with the 5-6K Interface Board. Before going to the ADS8363, can I ask if you are updating the DAC8331 at…
Shekar,
One additional item to consider - please refer to Figure 11 in the datasheet - the ADS8361 starts off from power up in mode 1. The output data from the first transfer could be from an either CHA or CHB. The state of the mode pins is determined …