Other Parts Discussed in Thread: ADS8342 , CCSTUDIO I have TI ADS8342 EVM board Rev. 2. I am trying to port data to TMS320C6713 DSK Rev D with 225MHz clock using 5-6K Rev B board. I am using CCStudio v3.1. I have tried to follow the Example for C6711 but still…
Other Parts Discussed in Thread: ADS8342 Hi,
I am trying to use the ADS8342 with the schematic setup according to help from a previous post here: http://e2e.ti.com/forums/p/10474/40988.aspx#40988
However, when I power the board up with -5V connected to…
Hello Jame,
The code we provided directly is what was shipped out to help test the THS1206EVMs when they were manufactured. It is was based on the ADS8342 as you noted with some minor changes for the THS1206. It was not intended to be a fully complete…
Part Number: MSP430F447 Other Parts Discussed in Thread: THS1206 , , ADS8342 , TM4C123FH6PM
Hello,
I received the MCU MSP430 Vs ADC THS1206 EVM source code from the ADC forum at the address below.
https:// e2e.ti.com/support/data-converters/f/73/p/911632…
Hi Jishnu,
No, you can not change the BW of internal LPF. Also, when you use this ADC to measure a high frequency signal (e.g. 15kHz), your signal will be attenuated and distorted by the LPF. There are two possible solutions:
1. Use an ADC with integrated…
Hi Diego, Please let me know if there is any comment on the above question. Regarding the ADC output data can I assume it be something like the one below (from ADS8342 datasheet). Best Regards kummi
Aditya,
That configuration for the ADS8342 would work. The ADS8342 has True Bipolar inputs that would allow for a input range from +2.5 to -2.5V range. Short the Common pin to ground, similar to the setup shown in Figure 1. Keep in mind that the ADS8342…
Hi again Akerb,
The input range to the ADS8342 is +/-Vref about GND, with Vref being +2.5V (typical). The minimum reference voltage is specified to be +2.0V and there is no option for a -Vref input on this part. If you were to take your +/-1V input signal…