Hi Future,
Since these are NDA devices, they are not stocked at Mouser or Digikey.
You may request for the EVM from the respective device tools folder.
https://www.ti.com/tool/AFE4405EVM#order-start-development
https://www.ti.com/tool/AFE4410EVM#order…
Part Number: AFE4490SPO2EVM Other Parts Discussed in Thread: AFE4405EVM , AFE4405 Hi,
I would like to know if there is possible method to read AFE4490SPO2EVM & AFE4405EVM data via USB port using Python script?
And the second question is:
What is default…
Hello Prabin,
I have recently received the AFE4405EVM evaluation kit and therefore decided to run some tests on it. As it has some interesting features for my application, I will use it from now on. I understand that this post does no longer belong in…
Hi TI Folks,
Good day to you.
I have AFE4405EVM's hardware on hand without supported software, Please advise how can I get the software as soon as possible.
After I purchased the AFE4405EVM, there was no supported software inside the parcel, then…
Part Number: AFE4405 Hi,
I am going to apply a calibration code which will first work on AFE4405EVM board and then will be implemented on my own embedded board. I have questions regarding duty cycle:
1. Does the calibration code(included in the AFE4405EVM…
Part Number: AFE4405 Hi,
I am about to design an AFE4405 based PR/SiO2 board, after seeing the datasheet, the following issues need to be clarified.
Could anybody advise?
1) Can I use a single 3.3V power supply for both TX_SUP and RX_SUP ?
2) To handle…
There is also an evaluation module that you can buy for testing. It is not cheap, but this is for those who don't have a lot amount of time for electrical or software engineering. www.ti.com/.../afe4405evm Alexey
Part Number: AFE4405 Hi,
I am now designing a circuit with a module which has 3 green LEDs and 1 PD.(The green LEDs are at one side of the PD, not at both sides.)
The module will be attached to AFE4405. To my knowledge, the 3 green LEDs shall be connected…