Part Number: AM263P4-Q1 Other Parts Discussed in Thread: AM263P4 , Hi team, For the part AM263P4 ,please share the asssembly soldring or refloew profile Regards Jayakeerthana P
Hi,
Jayakeerthana P said: The recommended tool and procedure for UART flashing.
You can first try with Teraterm (if windows) or minicom (in Linux) and see if you are able to load via XMODEM at 115200 baud rate.
Jayakeerthana P said: The required…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: AM263P4 Hi Team,
I am referring to the AM263P4 Safety Manual, where multiple diagnostic methods/mechanisms are listed theoretically (for example in the diagnostic tables with diagnostic method…
Part Number: AM263P4-Q1 Hello , The Register Addendum mentions that the TOP_CTRL_EFUSE_DEVICE_TYPE indicates whether the device is High Secure and doesn't classify it as HS-FS or HS-SE. However, in the SDK examples, it appears that the register is used…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: SYSCONFIG Hi Team,
As per the Register description, the Select line for selecting source clock for Corresponding RTI is follows below. The confusion is (0x444 - DPLL_CORE_HSDIV0_CLKOUT0 = 400Mhz…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: AM263P4 H iteam, Could you please provide a following detail on eCAP integration. Consider a two MCU A and B. MCU A generating a PWM for driver and MCU B should monitor a PWM generated by MCU A…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: AM263P4 Hi Team,
I am working on MCAN implementation on the AM263P4 LaunchPad with the following configuration:
Nominal Bit Rate: 1 Mbps
Data Bit Rate: 4 Mbps (CAN FD)
MCAN Instance: MCAN3…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: TMDSCNCD263P Hi Team, We're using the TMDSCNCD263P evaluation board and unfortunately the MCU (XAM263P4ASOKFZCZ) got damaged. We already bought AM263P4AFONFZCZRQ1 for our custom board, can we use…
Part Number: AM263P4-Q1 Hello Team,
As Discussed here: AM263P4-Q1: Spi_MainFunction_Handling available only for SpiLevelDelivered 1 and 2 - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
As per our understanding…