Part Number: AM26LS32A Other Parts Discussed in Thread: LM339 , TLV1814 , ISO7740 , AM26C32 , AM26LV32E Dear team,
The customer would like to use AM26LS32A for their Encoder application. Please review below customer question.
1. The absolute maximum…
Part Number: AM26LS32A Hi Team,
I would like to clarify if I can connect the differential input (ex. A1 and 1B) with a voltage difference of around 24V max. The recommended common-mode input is +/-7V but the max is +/-25V.
What is the possible effect…
Part Number: AM26LS32A Other Parts Discussed in Thread: AM26LV32 Hi,
Please let us know the maximum supported data rate (Mbps) of AM26LS32AIDR chipset.
Regards, Arun Gomathi R Hardware Design Engineer DATA PATTERNS INDIA LTD Chennai.
Part Number: AM26LS32A I have received information that AM26LS32AID is becoming PDN, and I need to consider alternative parts. Please answer the following questions.
*Is AM26LS32AID really becoming PDN (EOL)? *Is there a recommended alternative? Please…
Part Number: AM26LS32A Other Parts Discussed in Thread: AM26C32
Setup:
For the setup on the original part, the G is connected to +5VDC and the G-bar is connected to ground which translates to ACTIVE HIGH. Each of the input ports for each of the 4…
Part Number: AM26LS32A Hi,
Good Day.
The customer would like to know if both P/Ns (AM26LS32DMB and DS26LS32MJ/883) are exactly the same component. If not, what are their differences?
Please advise. Thank you very much.
Best Regards,
Ray Vin…
Part Number: AM26LS32A Other Parts Discussed in Thread: STRIKE Hi Team,
Customer found some AM26LS32A are damaged in their products. Based on FA analysis(IV curve), there are multiple pins have leakage.
We think EOS/ESD may cause this situation, and…
Other Parts Discussed in Thread: AM26LS32A , AM26C32 , AM26LV32 Hi team
The customer wants to convert the output (3 pairs of differential pulse signal: A+/A-, B+/B-, C+/C-) of incremental rotary encoder to single-end signal, which could be connected…
Part Number: AM26LS32A Hi TI expert
Now we are using AM26LS32A to TTL 5V system.
Please suggest if there is a similar product which can be used for 3.3V FPGA system.
Best regards,
Thomas