Part Number: AM2754-Q1 Hello:
Can you provide a Trace32 CMM script for debugging the AM2754-Q1?
After installing the latest version of T32, AM275X does not appear in the folder list for ARM-compatible hardware.
Thanks!!!
Part Number: AM2754-Q1 I have request access to AM2754-Q1 MCAL via link: www.ti.com/.../AM275X-RESTRICTED-SW
But It seems status is still access pending, could you help check if my request is received by TI support team?
Thanks.
Part Number: AM2754-Q1 1. Old board
- UART ROM boot outputs 'C'
- WKUP_R5F_0 is attachable
- SMS_CM4_0_TIFS_0 is NOT attachable
2. New board
- No UART output at all
- WKUP_R5F_0 reports WIR
- SMS_CM4_0_TIFS_0 is attachable
3. BOOTMODE…
Hi Andre,
AndreTseng said: This is totally unacceptable. Customer has design using 2xOSPI Flash by using both OSPI0 and OSPI1. and It's hard to explain why our software limit chip capability.
If we can not solve syscfg issue, we lose business.
As…
Part Number: AM2754-Q1 I am using the AM275 EVM, which includes HyperRAM. I need to know the starting memory address of the HyperRAM in the memory map. However, I could not find a memory layout table for the AM275 similar to the one available for the…
Part Number: AM2754-Q1 Hi,
I am using the C7x core of the AM2754. When the .cio section is placed in L2SRAM , there is no issue, but when it is placed in MSRAM , the following problem occurs:
Invalid CIO command (2) in the CIO buffer at address (0x80200000…
Part Number: AM2754-Q1 Hello TI,
We are using TIFS binary whihc is shared in
https://e2e.ti.com/e2eprivate/harman/harman_automotive/f/harman-sitara-mpu-forum/1625609/am2754-q1-am275x-hs_se-queries
Currently when using this we are facing issue while…
Part Number: AM2754-Q1 Hi! We are writing ARM and C7x code and running it on the AM275x development board. We are also in the process of producing our own board design using the AM27542AF, for use in our future products.
I am looking for the AM275x…
Part Number: AM2754-Q1 Hi,
I am using an AM2754 EVM. When I program the flash as described in the EVM setup guide and use OSPI NOR boot mode , everything works without any problem.
However, when I set the board to NOBOOT mode and try to connect to…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG Hi,
In the AM2754 stereo playback example, the number of buffers is set to four. Since it is essentially a simple talk-through example, I reduced the number of buffers to two. However…