Part Number: AM3351 We have to install new Linux kernel on AM3351 HS device.
The controller board was developed more than 10 years ago and the knowledge about signing and encrypting boot loader and kernel is not available anymore.
The processor marking…
Part Number: AM3351 Description: Our custom AM3351 board is configured with boot priority as SD Card → SPI0 NOR . The goal is to boot directly from NOR flash. The board does not include DDR, so we have optimized and reduced the SPL (MLO) size to fit within…
Part Number: AM3351 Team,
We are using OSD3358-512M-ICB, which integrates the AM335x Sitara™ Processor. I could not find the GPIO source/sink current specifications in the datasheet. Is there another document or application note that provides these…
Part Number: AM3351
Search term
Customer Part Number
Material
Material entered
PILZ
9904
74ALVCH32244ZKER
PILZ
187
ADS1248IPWR
PILZ
187.A
ADS1248IPWR
ADS1248IPWR.A
PILZ
5353
ADS7868IDBVR
…
Part Number: AM3351 Other Parts Discussed in Thread: TPS65218
Tool/software:
Using SDK9 with AM3351 and TPS65218D0PHP, how do I set the PMIC FSEAL bit using the TI-written driver?
*** 7/25/25: I'm updating this post to include my colleague's description…
Part Number: AM3351 Using the U-Boot 2026.04 release, I built a MLO file based on the am335x_evm_defconfig file.
Redoing the u-boot build using the 2017 Linux 4.9 product baseline ‘devel_am335x_defconfig’ file, the build fails with various ‘make’ pre…
Part Number: AM3351 Hi,
We are working on a design issue trying to connect an isolated USB connector to the AM3351 USB0 peripheral. Because they are galvanically isolated, we cannot connect the 5V VBUS signal on the connector directly to the VBUS pin…