Part Number: AM5718 Other Parts Discussed in Thread: SYSCONFIG Hi,
we have developed a custom board with an AM5718. Using SysConfig we have also determined the “best” pinmux configuration.
Yesterday, during software development on our board…
Hello John,
I could not since the original people working on those releases are no longer with TI. I suspect it might have to do with CMEM being deprecated.
See the following thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum…
Part Number: AM5718 Hello,
We are running a TCP socket server (TI-RTOS - NDK network stack) task on IPU2-Core0 and GMAC port 0 of the AM5718 SOC.
Recently we believe we may have observed an anomaly in our system related to a previous forum post linked…
Hello Jiablin, I believe this is a continuation from this thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1278293/am5718-low-singnal-on-porz-can-t-restart-the-linux-in-am5718-plat Can you confirm? -Josue
Part Number: AM5718
Hello there ,
I have used the SSC configuration for USB3.0 in the mentioned ticket ,
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/676452/am5718-usb3-0-spread-spectrum-clocking
I have done changes in …
Part Number: AM5718 Other Parts Discussed in Thread: DRA722 , TPIC2810
Hello ,
Greetings!!
i want to give the back ground of the work flow:
Yocto : dunfell (08.00.00.004)
Machine : am57xx-evm
Board : AM57IDK
kernel : 5.10.41-rt
Im currently facing issue…
Hi,
I was thinking from the perspective of if there is some communication required between phy and MAC to set up the MAC for communication at all and hence my question about the phy link status. But because its RMII, I am not sure if this could be a reason…
Part Number: AM5718 Hi,
I want to interface Grayhill 12 position channel knob PN : 513360-12-F with AM5718 processor.
The knob will give BCD output.
Which interface shall I use for interfacing and how to read the BCD value in processor.
Regards,
Khushboo…
Part Number: AM5718 Hi,
I have a custom AM5718 board. In this board we need to add wifi, Bluetooth and camera(4MP).
Kindly give the part number of wifi, bluetooth and camera to be interfaced with AM5718 for which software support like driver and interface…