Part Number: AM5726 Hello,
I'm working on a DSP program on the AM5726 where we're attempting to DMA data from a FIFO provided by an FPGA on the GMPC to L2 memory in the DSP. My understanding is that the SAM and FWID bits in the PaRAM options (and therefore…
Part Number: AM5726 Hi,
My customer has been doing tests in dual mac mode, related to the PPS signal. Following the guidelines provided in this link ( https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Industrial_Protocols_PTP.html#generating…
Part Number: AM5726 Other Parts Discussed in Thread: TPS659037 I want to power an AN5726 without GPU, EVE and IVA. According to SLIU011F page 4
I must connect the unused power pins to 1.06 V. Do I need to use the high current SMPS4 in parallel with SMPS5…
Part Number: AM5726 This is a follow up a thread originally posted by Tsurumoto regarding Isolation using AM5726.
Original post: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/983524/am5726-isolation
The ISOCLK_STATUS bit…
Part Number: AM5726
Hello,
I am working on an application where, after some initial setup occurs at boot, I want to prevent the DSP(s) from being able to access all but a small section of DDR memory. It seems like this might be possible using either…
Regarding the issues with IODelay Calibration:
Can you confirm that the sysboot14 pin is tied to VSS?
Also, can you confirm that all steps listed in TRM section "IO Delay Recalibration" are followed without any exceptions?
If there are no exceptions…
Part Number: AM5726 We are seeing an issue that seems to occur both in the TI AM5726 ROM code, and the associated Uboot image where the I/O isolation routine hangs waiting for the
The Technical Reference manual, section 18.4.6.1.7 "Isolation Requirements…
Part Number: AM5726 We have a design based on the AM572X EVM.
We are using a AM5726 processor and TPS6590378 PMIC.
The issue we are seeing is that in order to get the processor to boot we have to press power button immediately followed by the reset button…
Part Number: AM5726 Hello,
I am experiencing high network latency / spikes in latency at the moment a USB device is connected. I first observed this in a custom application but am also able to observe this with a simple ping
64 bytes from 172.31.4.205…