Part Number: AM5748 Hi,
As we could able to achieve the mailbox communication successfully between ARM and DSP1 cores on AM5748. The ARM Core is booted with Linux. The agenda of mailbox interface is to push the data from DSP1 to ARM on each second. DSP1…
Part Number: AM5748 Hi,
I am trying to test USB bulk transfer between AM57X and Linux host where AM57x is to be configured as a USB gadget via configfs.
I have refereed this link https://www.ti.com/lit/an/spracb5/spracb5.pdf for creating a USB gadget…
Hi,
We tried to implement SMP module for A15_0 and A15_1 of AM5748 processor and we are getting prints such that tasks are running based on the affinity.We implemented it using the JTAG by giving the Sync Group Cores.How is it possible to run the same…
Part Number: AM5748 Hi ,
I'am running RTOS MCASP audio example code in DSP core for AM5748 Custom board when I'm running this example using JTAG . we are seeing these prints below.
-------------------------------------------------------…
Part Number: AM5748
Hi TI Team,
We are using am5748 device, the GMAC support IEEE 1588 V2,
does Eth PHY also required to support IEEE 1588 V2 for time sync ?
presenlty we are using KSZ9031RNXIC Eth PHY that doesn't support IEEE 1588 V2.
Regards,
S…
Hello Arun,
This is not supported by our SW offering. When running Linux, you would have to use both cores of the A15.
For more information about bare metal support, also see the CSL library in RTOS SDK .
Part Number: AM5748 Hello,
We are using AM5748 in one of our design.
We are interfacing two Artix FPGA and one Spartan FPGA to the GPMC of the Sitara processor AM5748. Would like to know whether we need to provide a buffer at the output of AM5748 for…
Part Number: AM5748 Other Parts Discussed in Thread: TUSB320 , , TPS2051B
We are using usb with am5748. We run USB2.0 over USB-C using TUSB320. PMIC is not involved in Vbus detection.
The Vbus detection was suggested and reviewed by TI some time ago.
…
Part Number: AM5748 Hi,
I am trying to implement a socket programing that would communicate with the server of ip address 192.168.9.102.I am not facing any trouble with the code as it is not causing as crash.But i am not not able to see any packet transferred…