Part Number: AM62X-PET-CALC Other Parts Discussed in Thread: SK-AM62B-P1 Tool/software:
Hi,
We now want to port the jailhouse running on custom hardware. But we are not so familiar with this set of software, so we buy the official board first. The operation…
Part Number: AM62X-PET-CALC Tool/software: Dear TI support
I am new to u-boot and binman. We are working with TI team on secure boot image signing for TI customers. Our TI business contact told me that you used u-boot and switched to binam to build and…
Part Number: AM62X-PET-CALC Other Parts Discussed in Thread: TPS65219 Hello TI
We have a boot up issue in our newly project based on AM6232.I have taken the following actions.
1、 I have checked that the power on sequence of PMIC TPS65219 is correct…
Part Number: AM62X-PET-CALC Hello,
My Building Automation customer Fortune Brands had the following questions about a transfer of Sitara devices:
Can TI provide a brief explanation / bullet points on the complexity/challenges/process of porting embedded…
Part Number: AM62X-PET-CALC Hello
Has anyone ever encountered the problem of weston starting Qt and Qt popping up a Dialog will show in a random initial position
The problem is as follows picture: When Dialog is opened, the Dialog appears in a random…
Hi Daisuke-san,
Daisuke Maeda said: Was a heatsink used for the AM62x on the board used for measurements in the application note?
There was not one used. Instead a Thermal Flow System, TFS.
Daisuke Maeda said: What is the airflow (m/s) under temperature…
Part Number: AM62X-PET-CALC Hello TI Expert
In I2C specification , there are tf item listed , the min tf = 12ns when in Fast mode.
But in AM62x MAIN_I2C port , the tf can't meet >12ns requirement.
Can we modify the I2C output slope in AM6204?
…
Part Number: AM62X-PET-CALC Hello TI Expert
In RGMII specification , in my design we can't meet the min SRi = 2.64ns spec item.
We has tried to modify the ETH phy(88Q1110) into the max driver strength mode, and the test result is 1.8V/ns.
Any suggestion…
Part Number: AM62X-PET-CALC Hi TI
I use the Power consumption assessment sheet provided by TI.
When i select HS200 +Utilization 100%, but 0mA SOC_DVDD1V8 current result is show which not make sense, as the SOC_DVDD1V8 is connect to VDDSHV4 port which…
Part Number: AM62X-PET-CALC Hi TI
As you know , we can't test the SOC die side wavefrom but can only test the CSI nearest test point nearby SOC.
We found the waveform of CSI has non-monotonicity rising edge at nearby SOC side test point, whether this…