Part Number: AM62X-PET-CALC Hi TI
For the PWM signal generation, whether the EPWMxSYNCI is must connect pin to external CLK source?
Current desgin , i has no external Source can be used as EPWMxSYNCI, How can i use Sitara internal CLK source as EPWMxSYNCI…
Part Number: AM62X-PET-CALC Other Parts Discussed in Thread: TPS65219-Q1 , TPS65219 Hi TI
Can you help evaluate whether listed SOC is P2P compativable?
XAM6254ATGGGIAMC is p2p compatible with AM6204ATGFHIAMCQ1?
if any SOC peripherals design+ power design…
Part Number: AM62X-PET-CALC Hi TI
In the power estimation tool, how to selec the mode column list as below?what's the represent meaning of every item?when i used this port as GPIO which one can i select?
BR JINGCHENG
Part Number: AM62X-PET-CALC Hi TI
Can you support the stackup selection review?
Currently we use the attached 6-layer PTH stackup which is not same with EVM 8 layers.
1.LPDDR4 use a single die component.
2.System block is significant simpler than EVM…
Part Number: AM62X-PET-CALC AM6204 need support CAN RX function to recognition the CAN wake-up signal , Which power rail need connect to directly power rail?
BR Jingcheng
Part Number: AM62X-PET-CALC Hi TI
For AM6204 MCU_CAN port, there is no external pull up resistor added.
i want check the RX pin sink current capability , on the other hand please help check whether the external pull up resistor is need from TI view.
Belowe…
Part Number: AM62X-PET-CALC The GPIO has two domain in AM6204, Main domain GPIO / MCU GPIO , what's the GPIO assignment principal in HW schematic design ?
For example , CSI port control related GPIO ,may select from Main domain GPIO group or MCU GPIO…
Part Number: AM62X-PET-CALC in the SPRAD06 documentation , table 3-7 listed the Data Group Routing Specification.
My query is : LPDDR4 may support the write level function between DQS and DQ, Why the skew limitation need control to max 2p?
The spec from…
Part Number: AM62X-PET-CALC Hi TI
As the data sheet show , E14_RESTATz Pin is low status duing reset, and ss status after reset.
How can i check the SS status of E14?SS:The subsystem selected with MUXMODE determines the output buffer state.
BR Jing…