Part Number: AM6441 Hello,
I'm currently investigating on how to use the different cores of the AM64xx between real time and non real time processing. All cores should access to the Ethernet part with different priorities in both direction (Rx/Tx…
Part Number: AM6442 Other Parts Discussed in Thread: TPS65220 , TPS65219 , , AM6411 , AM6422 , AM6412 , AM6421 , AM6441
Hi TI Experts,
Can you provide a List of collaterals that can be referred when starting a custom board hardware design.
Hi TI Experts,
I am starting a new board design and planning to use TI EVM design files for designing my custom board. Please let me know if you have any suggestions.
Part Number: AM6441 Other Parts Discussed in Thread: AM3358 , Dear TI experts,
I'm currently migrating from a design based on AM3358 to one based on the newest family AM64x (in detail AM6441), and I'm facing a problem related to the ETH interface section…
Part Number: AM6441 Trying to understand the boot process from reading the TRM. Is it the R5 or the A53 that boots from the boot memories? (This is unclear to me?) Section 4.7 describes the image loaded from the OSPI interface as: "The image data (blob) is…
Part Number: AM6441 Hello TI team,
The newest design I'm developing is based on AM6441 Sitara Processor. At the moment I have to provide to our EMS the exact part number to mount on my PCBs, and I have a couple of questions in order to define it: …
Part Number: AM6411 Other Parts Discussed in Thread: AM6441 , SYSCONFIG Hello,
My customer is working for a prototype with AM6441.
At first, they used web version of SYSCONFIG to configure AM6441 pin mux.
Then they want to integrate this configuration…
HI Mike,
Michael Erdahl said: 2. If MMC1 is not used, CAP_VDDSHV_MMC1 still needs to be bypassed to gnd with 1uF cap per the datasheet.
How about VDDSHV5 pin?
When I checked in below datasheet, I thought VDDSHV5 should be connected to 1.8V or 3.3V even…
Part Number: AM6441
Hello There,
I was wondering if the CMEM driver module is supported on aarch64/arm64 platforms?
My use case is for setting up DMA transfers from an ARM Cortex M4/M5 Processor to/from ARM Cortex A53 Cores.
I have tried building the…