Laurent Joye said: The lonely difference with our own hardware board is that the TX lines are swapped to the opposite PRU slice, as documented for MII mode.
Could please confirm that the swapping is also working?
Yes the swap is needed.
Part Number: AM6548 Hi Ti,
We are using several PRUs in AM65. And from TRM, there are IEP0 and IEP1 inside.
And if there any standard to choose IEP0 or IEP 1 for specific PRUs?
Thanks.
Eric
Part Number: AM6548 Hi, I can't seem to find a link to apply for the NDA to get access to the security software and documentation for the AM65xx series. Could someone please provide me the link to apply? Thanks.
Part Number: AM6548 Hi Ti,
As you can see below, there is some code use #ifdef to separate different define.
Originally, I add EVM in Defined Symbols in Preprocessor, #ifdef EVM is WHITE, and #else is GRAY. It's no problem.
However, when I move EVM…
Part Number: AM6548 Hello,
Does the AM6548 support dual rank DDR configurations? We are seeing some conflicting information based on the technical reference manual. The technical reference manual says it supports up to 2 ranks for LPDDR4 only, while…
Part Number: AM6548 Hello, We are working to evaluate two Sitara processor-based SOM in one of our scratch design. We wanted to model power loss before actual integration into product.
Can you suggest ways to model thermal performance. Or can you send…
I am going to mark this thread resolved on my end since we are tracking offline. Feel free to respond to this thread to get it to pop back up in my inbox as needed.
Regards,
Nick
Part Number: AM6548 If have problems to debug the MMCSD bootloader provided by the Platform development Kit (pdk_am65xx_08_02_00_21). Building the SBL and running it from the SD-card with power up is ok (the SBL loads the application in my case GPIO_Baremetal_LedBlink_TestApp…
Part Number: AM6548 Hello,
Within the PDK for the AM6548, is there an CSL ECC example or test for DDR? It seems that the examples that come with the PDK are only for AM64x, SOC_J721E, or SOC_J7200. The ECC DDR examples under C:\ti\pdk_am65xx_08_02_00_21…