Part Number: AM6548 Other Parts Discussed in Thread: AM6526 I have a question regarding the issue we have when we try to boot the application with TI-RTOS for the R5 core. The problem is that the R5 application is not started at all.
My configuration…
Part Number: AM6548 Hello,
After installing the AM65x Processor SDK 08.06.00.47 and following the Getting Started guide to start building the SDK, I get the following error report when starting the bitbake command:
ian@pbcl-dsk7:~/Projects/P001295/TEMP…
Part Number: AM6548 Hello,
I am trying to figure out how to load remote firmware to the R5F cores of an AM6548 that is running a VxWorks kernel. I have been successful in loading the remote firmware (I think) using the following instructions https://software…
Part Number: AM6548
We are using one of the PRUs within the AM6548 to generate PWM signals using IEP compare timers. We are noticing occasional timing excursions with the global counter. Since this is used to generate the start of a 200 Hz frame on…
The latest is now in the AM64x Linux SDK 8.6 release . Note that the PRU firmware and Linux driver may have additional updates between now and the AM65x Linux SDK 8.6 release in about a month.
Regards,
Nick
Part Number: AM6548 Hi,
We got below error print by the kernel when using eMMC RPMB on AM6548:
```
[ 707.209027] mmc1: Got data interrupt 0x00600000 even though no data operation was in progress. [ 707.217640] mmc1: sdhci: ============ SDHCI REGISTER…
Part Number: AM6548 Hello,
Do anybody know what the maximum frequency for the 4 following PCIe clocks in an AM65 processor are?
PCIE0_FICLK
PCIE1_FICLK
PCIE0_CPTS_RCLK
PCIE1_CPTS_RCLK
BR
Trond
Part Number: AM6548 Hi Team,
Customer is using Linux SDK 8.2 for AM6548--They are trying to use the PRU to auto-forward packets from RX0 port to their TX1 port. Ideally, they'd like to use the AM65x as a sniffer on this comms line.
This auto-forwarding…