Part Number: AM6548 Hi Ti,
We are using AM6548 with Linux RT SDK 7.
We want to know if Linux kernel support BPF Type Format (BTF) in any SDK?
If any SDK support this, how to configure and compile kernel with BTF enable?
Thanks.
Eric
Part Number: AM6548
Hi Ti,
On AM6548, we tried to read/write ASIX AX58100 by SPI.
From the waveform capture as attached, I can see some data output from AX58100.
In below pic, C2 is MOSI, and C4 is MISO.
And the " RED " square is the data from AX58100…
For future readers, we are continuing the conversation about not getting an IP address from the DHCP server on thread https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1158425/am6548-icssg-ethernet-driver-crash
Regards,
Nick
Please would you also explain exactly the meaning of the following fields in the MII G RT FDB CFG1 register:
FDB_HASH_SIZE - is this related to the number of broadside slot entries? does it have to match the mask (e.g. 0x1ff) used to convert the CRC…
Part Number: AM6548 Other Parts Discussed in Thread: AM6528 , UNIFLASH Hello all,
I want to write/download code in Single-SPI-Flash (EVM's SPI NOR Flash MT25QL128ABA8E12; processor AM6548/AM6528) for development and later mass production purposes. …
Part Number: AM6548 Hi,
I'm trying to boot my AM648 EVK board from the MT35X NOR flash on OSPI. Currently the situations is:
- I was successfully able to generate a .wic with yocto. - That .wic, once flashed on an SD card, boots normally. - I added…
Part Number: AM6548
Hi Ti,
Do you have any further information of "PADCFG_CTRL0_CFG0" of AM6548?
I can find it in AM64 TRM but not in AM65. Below is the screen shot from AM64.
Or is there any other document related to this?
Eric
Part Number: AM6548 As a follow-up to several related issues running the PRU-ICSSG networks on custom board with a third-party OS+custom driver, we've run into yet another issue.
Our driver has been ported to support the more recent versions of the…
Part Number: AM6548 Hi Ti,
We are using Linux RT SDK 07.01.00.18 on our customized board and tried to check the behavior of MDIO.
We connect a mdio with a ethernet phy, Ti83867.
&icssg1_mdio { status = "okay"; pinctrl-names = "default";…
Part Number: AM6548 We have 3 sorts of AM6548 Board for our customer.
The two sorts of products work well for silicon migration rev2.0 to 2.1
But one product doesn't start.
I checked the hardware. I think the basic problem is WKUP_OSC Crytal.
The…