Hello Kevin,
I found this thread but not muh information.
(+) AM6548: HDMI support - Processors forum - Processors - TI E2E support forums
We have the DPI signals on a connector. Not sure if the interface was tested.
We have the HDMI implementation on…
Part Number: AM6548 Dear TI Support,
After I run the /etc/init.d/rc.pvr start command to initialize the GPU, I am getting a few error messages printed to the screen:
root@tqma65xx-2gb-mba65xx:/etc/init.d# ./rc.pvr start
PVR:(Error): PVRSRVDetectPlaform…
Thanks TI engineers' help, we had solved this issue, it's a SERDES0 lane select issue:
It's from board/ti/am65x/evm.c in uboot source code:
/* * It has been observed that setting SERDES0 lane mux to USB prevents USB * 2.0 operation on USB0…
Hi,
This looks to be kernel configuration issue related to bluetooth and not the TI device or drivers. Please check your kernel configuration to see if features related to RFCOMM and Bluetooth are enabled.
Best Regards,
Schuyler
Part Number: AM6548
We're migrating PRU code from the AM335x processor to the AM6548 and noticed that the Mailbox 0 constant table entry (22) was removed in the AM6548 so it is no longer available in the PRU/RTU local memory space.
We are looking…
Part Number: AM6548 Other Parts Discussed in Thread: STRIKE [Follow-up to AM6548: PRU ICSSG (SR 2.0) receive stalls .]
Since the last activity reported on the "parent" thread, we have:
updated the host driver for PRU-ICSSG EMAC to work with the…
Hi,
Here some answers to your questions:
Q1.I think DP83867 does not have the function to output PPS signal from GPIO. Is this understanding correct? That is correct, the itself will produce a PTP signal.
Q2.Judging from the diagram in the PTP using ICSS…
Part Number: AM6548 For debugging it is necessarry to disable the M3 watchdog. This works fine but i can't find a comlete register desciption in the AM65x/DRA80xM Processors Technical Reference Manual. Where can i find a description of these registers…
Part Number: AM6548 Other Parts Discussed in Thread: SYSCONFIG Hi Support Team,
AM6548 device that can be selected with SysConfig(1.12.1_2446) is the beta version "AM65xx_SR2.0_beta". When is the planned release date of the SYSCONFIG that allows…
Part Number: AM6548 Other Parts Discussed in Thread: SYSCONFIG
Hello,
I am working on a system based on AM6548 in which a subset of the Cortex-A53 cores will run in TrustZone secure state. (This approach was recommended by TI to support use of the hardware…