Part Number: AM6548 Hi TI experts,
I've been experimenting with the USB driver code that is available through RTOS SDK of processors like am65, am57, etc.
I had some success enumerating a flash memory device that was communicating at high-speed . Unfortunately…
Part Number: AM6548
Hello,
The board_internal.h is missing from both the am65xx_evm and am65xx_idk sources under ti/board/src/... It exists for the other boards in that directory.
It is included by am65xx_idk.c (and am65xx_evm.c) file for compilation…
Hi Krunal,
Finally got it working today!
Long story short, it was just building those two packages, and running the /etc/init.d/rc.pvr start command before running the kmscube application. I am now averaging about 120 FPS, which is a lot faster than 4…
Part Number: AM6548 Hi TI,
I'm currently using the System_printf function to log messages in the R5F. I was wondering if there is an easy way to add timestamps to my prints.
This would help log execution time and waiting time for different functions…
Part Number: AM6548 Other Parts Discussed in Thread: DP83640 Hi Support Team,
Is it correct to understand that the combination of AM6548 and DP83640 can enable IEEE1588v2 (PTP) to realize high precision system synchronization function?
The following forum…
For future readers, we are continuing to discuss both the DHCP server / no RX packets issue and the kernel crash in this other thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1158425/am6548-icssg-ethernet-driver-crash …