Part Number: AM6548
I have a question about synchronizing the timestamps between ICSSG slice 0 and slice 1. My end goal here is synchronized packet capture between slices and hopefully PRU instances. I am running the icssg-prueth firmware in all PRU…
Part Number: AM6548 Hello,
I am looking to drive an external circuit with the AM65x_GP_EVM. I cannot seem to find any GPIO breakout or test headers on the board itself. Did I miss something when reviewing the design? Or could I possible repurpose an existing…
Part Number: AM6548 Other Parts Discussed in Thread: DRA829J Hi experts,
Is there any plan to support (fix) LCPD-20006 in the next version of the SDK?
This is a continuation of the original thread and my customer is asking to share the status. I am aware…
Part Number: AM6548 Other Parts Discussed in Thread: TMDX654IDKEVM if order TMDX654IDKEVM now, Is the application board E4 version?
Can only order a E4 application board?
https://www.ti.com/tool/TMDX654IDKEVM
Hello Daisuke-san,
I have added a note to the bug report asking the developer to let me know when they start working on this issue. When they ping me, I will unlock this thread (if it has been longer than a month) and provide you with an update.
Regards…
Part Number: AM6548 Hi,
We have same issue on AM65x-EVM board with HSR + PTP... We are following instruction from https://software-dl.ti.com/processor-sdk-linux/esd/AM65X/latest/exports/docs/linux/Industrial_Protocols_PTP.html#redundancy-hsr-prp
It is…
Ok, so the AM65 has a signgle CPSW2G and 3x PRU_ICSSG. My question regarding the PRU_ICSSG remains: is each PRU_ICSSG bottlenecked on the internal side even when running in dual mac mode?
Part Number: AM6548 Other Parts Discussed in Thread: SYSBIOS Hi experts,
Please allow me to confirm a few things about the OS of A53 on AM65x.
Q1:Which of the following methods do you recommend when proceeding with development with TI-RTOS (SysBIOS)?
…
Part Number: AM6548 Hi Team,
we would like to use SERDES0 as USB3 interface. For this the TI EVM implements an external clock source CDCI6214RGET.
Can't we use REFCLK0P/N and connect it to SERDES0_REFCLKP/N, or is there an issue with the frequency/jitter…
Part Number: AM6548AM6548 has 5 UARTs as shown below, can they all be used together on Linux?
WKUP_UART0 MCU_UART0 UART0 UART1 UART2
In the DT configuration example below, only up to 4 UARTs are used.
software-dl.ti.com/.../UART.html
Best regards,
Daisu…