Part Number: AM6548 Hi Ti,
We are using Linux SDK, and we want to lower eMMC speed for some test.
However, when I modified the dts as below, the eMMC speed still not changed.
Please let us know how to do this in uboot and Linux.
sdhci0: sdhci@4f80000…
Part Number: AM6548 Hi Ti,
Our EE engineering met an issue that AM6548 boot fail when during test with -20 degree C with our customized board.
Below is the fail log. The fail rate is about 25%.
We want to know:
1.Where the EL3 is? In the SPL or uboot…
Part Number: AM6548 Hello,
I am working on an AMP system design using AM6548. As suggested by TI, one core of the AM6548 runs in TrustZone secure world, whereas other cores run in TrustZone non-secure world.
The secure (primary) core starts first and…
Part Number: AM6548 Other Parts Discussed in Thread: TMDX654IDKEVM Dear TI team,
We are using the PROCESSOR-SDK-LINUX-RT-AM65X "Version: 08.06.00.47" to generate the Linux image for our custom board.
We have found that processes using the AM65x…
Part Number: AM6548 Other Parts Discussed in Thread: TMDX654IDKEVM Hello,
I am using a AM65x_GP_EVM with SR1.0, I am attempting to use PRU ICSSG2 port 0 to use the PRU/RTU firmware binaries to load data over U-boot. I am following a similar process to…
Part Number: AM6548 Hi TI,
SDK : 8.02
We have connected 5 devices on I2C bus 5 (main_i2c3) on AM654 controller. We have connected 5 EEPROMS on this. EEPROMS are properly getting detected in uboot on power cycle and also on runtime if we remove or add…
Part Number: AM6548 Hi Ti,
Our EE engineering tried to test our AM6548 with low temperature. When the temperature goes to -20 degree, the device shut done.
And we tried to reboot the device, the log seems stop at SPL, and not go to uboot.
However, when…
This is a continuation of the discussion at e2e.ti.com/.../am6548-sbl-doesn-t-load-appimage-from-pdk-example
Hello Nick,
I am also not familar with the PCIe, and a search in the device tree files found no MSMC reference, probably PCIe drivers use unused…