For future reader, instead of reading the pinned reply, you can also refer to:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1298904/am6548-sbl-doesn-t-load-appimage-from-pdk-example/4960458#4960458
In which you may find something…
Part Number: AM6548
PRU Ethernet in U-Boot did not work on AM65x Linux SDKs 8.x. The feature is documented for SDK 9.1: https://software-dl.ti.com/processor-sdk-linux/esd/AM65X/09_01_00_01/exports/docs/linux/Foundational_Components/U-Boot/UG-Network.html#booting…
Nick Saulnier ,
Let me answer your questions.
1. Yes, there is a gold capacitor connect with RTC. Just think about a scenario, when CPU power off suddenly during accessing RTC. In such case, CPU is off but RTC does not. RTC might think there is someone…
Hello Pratap,
if a call is not possible, what should be the next step to be done to analyze the issue?
For testing purposes Novica configured the WKUP_UART at the beginning in main() of the flashwriter application to check if main() is started, but there…
Part Number: AM6548 It has been said that "the extensions *.ser5f *.aer5f *.oer5f have the usual meaning as *.s, *.a and *.o with the added suffix of r5f or a72fg or other core names. " . However, I'm wondering what does the "e" in the suffix means…
Part Number: AM6548 Hello,
we are using AM654xEVM with the AM6-IDKAPPEVM , running FreeRTOS, all in the ccs1210 IDE.
In future we have to use the Keil C CompilerKeil for developing SW on that platform.
Is there a description or can somebody help to change…
We now have ARM processor with 4 and 8-port hardware Ethernet switch parts available, https://www.ti.com/product/DRA821U (4 ports) and https://www.ti.com/product/AM69 (8 ports).
Part Number: AM6548
Hi,
I'm trying to do manual loading of LED blink example at u-boot prompt, the load has successed, but the R5 doesn't seem to work (the LEDs didn't blink and UART has no output) after issuing "rproc start 0" (no error reported), Is…