Part Number: AM6548 Need clarification on how we can test our PCBAs with a AM65 HS Sitara via JTAG boundary scan.
There could be different possibilities: 1. First test the board via boundary scan with a HS-FS device (before key programming), then do the…
Part Number: AM6548 Hello,
On page 144 of the datasheet "AM654x, AM652x Sitara Processors Silicon Revision 2.1 datasheet (Rev. B)", Figure 7-4 has labels such as "Note 6" and "Note 10" (screenshot below)
However, I am unable…
Part Number: AM6548
Hi,
I have been experiencing similar clock jump issues as described in thread:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1235566/tmdx654idkevm-tmdx654idkevm-clock-jump-of-ptp-device-for-icssg-2
I am…
Part Number: AM6548 Dear,
Sometimes our AM6548 based device could not boot from u-boot SPL to u-boot proper:
NOTICE: BL31: v2.6(release): NOTICE: BL31: Built : 08:03:39, Oct 20 2022 I/TC: I/TC: OP-TEE version: 3.16.0 (gcc version 10.2.1 20210110 (Debian…
I went through the NB registers and specs and it looks like it will pass through the secure or not sideband information from the initiator. From caching perspective the secure bit is still basically like an extra address bit, so address + secure/not is…
Part Number: AM6548 Other Parts Discussed in Thread: SYSBIOS , Hi everyone,
I am facing a problem in debugging basic bare-metal example on Cortex-R5F core (MCU1_0) of AM65xx IDK board. My environment setup consists of:
- Code Composer Studio v12.40
- AM65xx…
Part Number: AM6548 HI all,
I am seeing higher voltage 3.3V at CAP_VDDSHV_SDLDO instead of 1.8V.
Any solution or idea to control these voltage
part used :XAM6546ACDXEAF M4
I was running memtester today on an AM62A board that has more than 2GB of DDR (4GB, to be exact) and was able to use it without issues as follows:
root@am62axx-evm:/opt/edgeai-gst-apps# free -h
total used free shared…
Part Number: AM6548 Hi,
Regarding USB3.0 SSC function of AM6548, we've tested it on previous project, which has a USB3.0 connector.
On our new project, there's no USB3.0 connector, mini-PCIe card will use USB3.0 lane.
Since they utilize same serdes…
Part Number: AM6548 This is to bring attention for the LKML bug report and its related questions about the affect processor to this forum:
https://lore.kernel.org/lkml/e0bc7eb5-f1b9-4e99-a39f-ca6f31daa9d8@siemens.com/T/#u
Can someone confirm if that powering…