Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507 , AMC131M03 , SYSCONFIG Tool/software: Hi,
Shortly about the setup: MSPM0G3507 launchpad connected with wires to AMC131M03 EVM, the code is based on the TI examples and is using…
Part Number: TPS74801 Tool/software: Hi team,
Would you please help us below transient test waveform if you have TPS74801 EVM on hand?
Vin 1.8V to Vout 0.9V, 0~1A, 50A/us slew rate(if your eletric load can support this slew rate)
Thank you!
Hi Dakshina,
I was able to locate an EVM, I'll make some time for the test and mods and come back to you by the end of the week.
Best regards, -Ivan Salazar Applications Engineer
Hi Jayarafj,
You can use the LM5137 quickstart calculator to estimate losses, as it depends significantly on Vin, Vout, Fsw and power stage component selection.
https://www.ti.com/tool/LM5137-LM25137-DESIGN-CALC
I have tested the controller to…
Part Number: TPS25763Q1EVM Tool/software: We have the TPS25763Q1EVM for evaluating the ability to charge a tablet while supporting data. The tablet is plugged into J30 and charges properly. We have a laptop plugged into J29 on the EVM. We have tried a…
Part Number: AMC7834 Tool/software: Hi team,
My customer is evaluating AMC7834 on the prototype board. He's struggling to read out current sense registers on address 0x28 - 0x30.
The register configuration below is set to default.
ID
…
Part Number: LMG3100EVM-089 Tool/software: What is the maximum output current of this EVM board? I am looking for a buck converter module with current output rating of 50A when operated with Vin 10V and Vout = 4V? I will appreciate all your recommendations…
Part Number: BQ76952 Tool/software: Hello TI Team,
We are developing a 16S, 50A Li-ion BMS using the BQ76952 and would appreciate your feedback on our schematic and PCB. The design incorporates external N-channel MOSFETs for cell balancing (VCn–VCn…
Hi Neil,
Neil Wilson said: Building from ti-processor-sdk-linux-am62xx-evm-10.01.10.04 with these mods:
Could you please give it a try with SDK 10.00.07.04? From some past testing I've done with SDK 10.01.10.04, I saw some issues with Ethernet boot…
Well, I must admit that some recommendations come from the intuition or experimental results. In some AMCxxxx device datasheets or EVMs you may see ferrite beads. They often improve EMC behavior as the modulator sampling (the input of the AMC device)…