Part Number: TMS320F28375S Other Parts Discussed in Thread: AMC1303E2520 , AMC1306E25 , AMC1303M2520 Hi,
I have a 3 phase PFC application. I measure 3 phase currents, 3 phase voltages, dc voltage and dc current. The 3 phase voltages are "smooth" 50Hz, the…
Part Number: AMC1306E25 Other Parts Discussed in Thread: AMC1303E2520 , SN6501 , AMC1303M2520 Hi,
so this is a sort of a continuation of my previous post:
e2e.ti.com/.../2644974
but as I have now discovered that it is probably not the C2000 problem and…
Part Number: AMC1306E25 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello, I'm trying to use AMC1306E25DWVR for DC link voltage sensing of the inverter. Where I can find this model for simulating my circuit in Tina…
Part Number: AMC1306E25 Other Parts Discussed in Thread: TMS320F28377D According to the datasheet of the AMC1306E25, it should respond to the clock at first by printing a test pattern, then the output data channel will stream invalid data for (t ASTAR…
Part Number: AMC1306E25 Recommended Modulator Clock
Evaluating AMC1306 (first prototype series) - we see some problems concerning stability of this part.
Running with somewhat 16MHz on CLKIN - we see artefacts on heating up the device.
Isolating the problem…
Part Number: AMC1306E25 Other Parts Discussed in Thread: TMS320F28374S , AMC1200 , AMC1303E2520 , AMC1303E2510 Hi,
I'm starting a new project and I'm switching form Microchip to TI C2000 Delfino class probably to the - TMS320F28374S. I already used…
Part Number: AMC1306E25 Hi, I don't understand about the density of ones in the output bit stream.
If there are ten 1s in 100 bits, so the density is 1/10. It's also possible that we can see two 1s in 10 bits, so the density changes to 2/10. What…
Part Number: AMC1306E25 Hi,
I'm making a 3 phase buck converter and I need 3 phase current measurements (1 for each phase) and 1 voltage measurement (output voltage).
In my current schematic I have it set up so that the current measurement is between…
Jens,
Sorry for responding late. I think I found root cause of your problem.
It looks like AMC1306E25 manchester encoded bit stream gives LOW to HIGH toggle pulse for a '1' and HIGH to LOW toggle pulse for a '0' whereas F28377S seems to support HIGH…
Other Parts Discussed in Thread: TMS320F28377D , AMC1306E25 , AMC1306M25 circuitous philosophy:
Logic block diagram:
Question 1 .AMC1306E25 is compatible with TMS320F28377D.
Question 2. How should TMS320F28377 be configured and Select "SDFM Electrical…