Part Number: AMC1306M25 I want to use the Simulink model of AMC1306 for system-level simulation, but I can only download the IBIS model from the device webpage. How can I obtain or request the Simulink model for this device?
Part Number: AMC1306M25 Hi,
What is the UL number of AMC1306M25DWVR? Is it number for UL-US-L181974-14-02604102-3 on the attached file?
Please help to confirm, thanks~
sbaq007-amc1306.pdf
Hi Alexander,
Thanks for your reply. Customer tried implementing all the recommended suggestions but the saturation issue still persists. Please find their comments below.
1. When we individually test the IC with +/- 250mV at the inputs, we are getting the…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1305M25 , Hi,
in the datasheet of AMC1305M25 section 7.10 is shown Vclipping with 312.5mV Typ.
For AMC1306M25 it is shown with 320mV.
Are both values correct, if yes what's the reason for the…
Part Number: AMC1306M25 Hi team,
What is the flammability rating of AMC1306M25? I didn’t find it in the datasheet. Do you have related materials?
Really appreciate your help!
Thanks & Best regards,
Wendy
Part Number: AMC1306M25 Hi Team,
Could you pls recommend suitable device of two-channel buffer for CLKIN and DOUT pin in AMC1306M25 device? Thanks.
Best,
Stanley
Part Number: AMC1306M25 Hi BU:
I have one issue about the AMC1306M25 and need your help.
Customer evaluate the performance of AMC1306 in the high temperature. Please see the below picture.
The red is the actual current waveform , and blue is the sigma_delta…
Hi Hui,
1.) Both the AMC1204 and the AMC1306 should have the AGND (pin 4) of the device connected to the shunt. I don't believe that is specifically spelled out in the AMC1204 datasheet, but that is the general intention depicted in Figure 50 of the datasheet…
Other Parts Discussed in Thread: AMC1306M25 , AMC1204 The schematic diagram is as follows:
After sampling with AMC1306M25 oscilloscope test motor U phase and V phase waveform is as follows:
You can see spikes in both phases;
Same program and hardware…
Part Number: AMC1306M25 Hi
I want to test F280049 SDFM with AMC1306M25 on a universal PCB board, I bought some SOIC-8 to dip
adapters but SOIC-8 dimensions are different to the ones described on AMC1306 data sheet.
I checked SOIC-8 package on internet,…