Part Number: BQ24022 I am trying to test the BQ24022 charging IC and checking the operation flow chart I am quite certain that the requirements have all been met for the IC to begin charging from a USB input but I am not seeing a rise on the STAT1/2 pins…
Other Parts Discussed in Thread: BQ24022 Hi everyone,
in our devices we're using BQ24022 as a battery charging IC, to charge the LiPo battery.
It is a consumer device and under some circumstances while charging, the BQ24022 falls into an undefined…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ24022 Hi,
We have altered the ZVCHG Exit Threshold value from it's default value (2200mV) to 0mv (Zero).
This appears to effectively stop charging from a cell voltage of 970mV all the way…
Other Parts Discussed in Thread: OMAP-L138 , OMAPL138 , TWL6040 , PMP , LP3971 , BQ24022 , TPS65023 Hi,
I am using OMAP-L138 LCDK.I need to use UART0 and UART1 in my application to be be ableto perform this I needed to change some lines in arch\arm\mach-davinci…
Do you mean a bq24022 internal regulator driver? Would you point out which regulator driver is from the function block diagram of bq24022 datasheet?
If it is not a bq24022 internal regulator driver, is it designed in in the mainline linux-kernel developed…
Hi,
for devices connected via GPIOs it seems the way to go is via a machine-info struct which is filled with the correct GPIO-information in the board-definition. See drivers/regulator/bq24022.c, include/linux/regulator/bq24022.h and the corresponding…
Other Parts Discussed in Thread: AM3892 , DAC7512 , PMP , TPS65010 , TPS65910 , BQ24022 , LP3971 , LP3972 , TPS65023 , TLV320AIC23B , TVP5150 , TVP7002 , THS7303 , DA8XX Hello,
I have custom board, based on TI am3892 processor. I managed to load Linux kernel + Arago…