Hi David,
Yes, for BQ24095 Vhot = 0.278 V , Vcold = 1.23 V.
Customer is finding 0~45C, standalone, no JEITA, up to 0.35A charge current, 4.35V regulation device. BQ24095 meets these requirements. A power-path device that also works here is BQ24232H. …
The host/UFP port provides up to 500mA/900mA depending on USB 2.0 vs 3.0 requirements and your device is required to be at or below this level of current. If you only draw 100mA, you will be within the UFP limits.
If you are a device, then there is…
If I look at the bq24232H I'm confused by the Vin spec. It has a line that says Vin can have a max of 26V but then the line below says operating voltage range of only 10.2V max. Are they just trying to say that you can have spikes of up to 26V but the…
Haresh,
BQ25100 is a good choice for charging. If you need powerpath to support system load, you might consider BQ24232H.
If you need additional rails for a DC-DC or LDO and I2C programmability, you might consider BQ25120.
regards,
Gautham
I set up a bq24232H EVM with your configuration and tested the termination function and /CHG output.
Did not see any problem, charge will complete right at 48mA and /CHG pin will transition from low impedance to high impedance.
Also noted that the pin…